Beli kertas anti karat di monotaro.id

Kami Menampilkan Rekomendasi Kami Untuk Anda! Anda Bisa Membelinya Kapan Saja di monotaro.id
  1. ARMOR Protective Packaging Kertas Anti Karat
    Mulai

    Rp4.199.900

    ARMOR Protective Packaging Kertas Anti Karat
    Deskripsi:
    ARMOR WRAP® 30GProduct OverviewAll Armor Protective Packaging® products utilize our proprietary and time-proven ARMOR vapor corrosion inhibitor (VCI) Nanotechnology®. Oxidation occurs when an electrolyte (water, oxygen, etc.) is present on the surface of a metal. The corrosion process begins when electrons flow through the electrolyte from high energy areas (anode) to low energy areas (cathode) of the metal. ARMOR VCI blocks this reaction by passivating the surface and inhibiting the electrochemical current flow from anode to cathode. ARMOR VCI’s protective vapors adhere to a metal surface to form an invisible film only a few molecules thick to protect metal from attack.ARMOR WRAP® 30G paper is a 37# total weight (paper and VCI Chemical) neutral pH, natural Kraft paper impregnated with Vapor & Contact Corrosion Inhibitor (VCI/VPI) formulation for ferrous and non-ferrous metals. ARMOR WRAP is designed for long-term storage of metals. ARMOR WRAP is both Sodium Nitrite and Calcium Chloride free.Shelf Life & Storage of ARMOR VCI ProductsWhen ARMOR WRAP® VCI paper sheets are stored properly (nested together and wrapped or in some sort of closed container), the shelf life is two years from the date of manufacture. Due to the way VCI is emitted fromthe packaging material, ARMOR WRAP VCI paper rolls have a longer shelf life of up to three years when stored properly. VCI papers are hygroscopic (absorbs moisture from the environment) so it is important to store in original packaging or enclosed inside a container. After VCI paper has been exposed to the atmosphere for a period of 24 hours, please remove the outside layer of paper from a roll or the top four sheets from a stack ofcut sheets and dispose of them prior to using the rest of the product.For best results, do not leave ARMOR VCI packaging out in an open environment, either indoors or outdoors. Keeping it in its original packaging or enclosed inside a container ensures that the vapors remain in the packaging. As temperature and humidity levels increase, the rate of the volatilization of the chemicals contained in the packaging also increases, reducing the effectiveness and longevity of the product. Product should be stored in a dry environment with temperatures between 40° – 110° F (5° – 43°C).Note: While Shelf Life and Length of Protection are two separate characteristics of VCI packaging materials,they are somewhat interrelated. Shelf Life refers to how long the unused VCI packaging material can bestored prior to being put in use. Length of Protection refers to how long the VCI packaging materials provide protection once in use. In both cases the duration depends on the product’s storage conditions.ReusabilityARMOR WRAP® is not recommended for re-use for three primary reasons:1. The rate at which VCI chemical volatilizes out of the product into the surrounding environment when in use2. The inability to properly track and monitor the amount of time the materials have been exposed to the environment3. Potential contaminants on the packaging that can be transferredFor those instances when re-use is necessary, be sure the packaging is free of dirt, holes, or other contaminants. Once these factors appear, it is best to use new, clean ARMOR VCI packaging. It is also important to note that the length of time the packaging material has been exposed to the environment (especially high heat/humidity) will greatly impact the effectiveness of the product. Do not re-use VCI packaging more than two times. Please note, ARMOR cannot guarantee the amount of VCI that remains in the packaging upon re-use.Length of Protection & Long-Term StorageARMOR VCI products are used to cover or wrap metal parts and surfaces. The continuous vaporization of this chemically treated packaging creates a safe, protective environment that effectively blocks out rust, corrosionand oxidation. Typically, ARMOR VCI packaging will protect parts for approximately three years of corrosion-free storage when used properly in normal warehouse conditions. However, by following the guidelines, it is possible to lengthen this time-frame considerably. The key element in protecting parts for long-term storage is that thepart must be completely clean, prior to wrapping in ARMOR products. We recommend that parts be completely wrapped or enclosed in airtight packaging for best results and longest protection time.ARMOR cannot control variable conditions such as temperature and humidity extremes, airflow, production and process methods, surface conditions of metal to be protected, customer employee training and other factors beyond our control, therefore it is impossible to guarantee a specific length of protection. Additionally, if warehouse conditions are expected to be severe (i.e. over 90 F and 75% RH) for any length of time, other methods of rust preventatives such as Dry Coat™ RP or desiccants, may be needed, in conjunction with VCI packaging. Successful long-term storage requires that all of these guidelines be met. It is important to test parts and packaging as extensively as possible, prior to conducting any long-term storage projects.
  2. Multiguard VCI Anticorrosion Film
    Mulai

    Rp1.999.900

    Multiguard VCI Anticorrosion Film
    Deskripsi:
    - Product Characteristics.MULTIguard is a kraft paper combined with the basic VCI quality of BRANOpac. By constantly emitting a small amount of active anticorrosion substances (VCI principle: Volatile Corrosion Inhibitor), MULTIguard papers help to protect metal parts during transport and storage. Active VCI agents effuse and build up a protecting atmosphere, which protects reliably against rust, even after having opened the package for a short time - the protecting atmosphere can be rebuild immediately. MULTIguard works both in contact and from a distance. MULTIguard can be used as a simple single wrap, interlayer or lining material. For basic applications in production, storage and shipping. - Development of the Protective Atmosphere. The distance between MULTIguard paper and metal depends on the package volume and the time permitted for a protecting atmosphere to build up. A rule of thumb: for steel, a full protection is achieved at a distance of 30 cm after 15 minutes, for copper and alloy, at 12 cm and after 24 hours. Cast iron is only protected on contact. The air tighter the package, the longer the protection will last. Advantages : - Environmentally friendly corrosion protection based on paper. - Metal parts are ready for use at any time. - Oiling and greasing aren't necessary anymore. - Economy of time. - Package and anticorrosion protection together. - Simple disposal. - Low package requirements. - In accordance with TRGS 615. - Marked with the Resy label. - Represents no health hazard. - BRANOpac is certified according to ISO 9001 and ISO 14001. Range of Protection. According to your application, basic VCI papers are available in different performances (RUM formula). R Ferrogard protects steel, cast iron and iron reliably. Be careful with zinc, nickel, cadmium, lead, soldering tin, magnesium, wolfram, molybdenum, copper and its alloys. U MULTIguard protects steel, cast iron (only on contact), zinc, copper, chrome, bronze, brass, pure aluminium, pure tin reliably against corrosion. Be careful with Cadmium, lead, soldering tin, magnesium, wolfram and molybdenum. M Ferrogard M, same as Ferrogard, but without nitrite.
    atribut:
    • Size (m): 1x100
  3. ADPACK VCI Paper Single Sheet ASK - 6M
    Rating:
    100% of 100
    (1)
    Mulai

    Rp20.900

    ADPACK VCI Paper Single Sheet ASK - 6M
    Deskripsi:
    Adpack-S (Impregnated for Ferrous & Non-Ferrous)Impregnated type for Iron & Steel, Non-Ferrous productsIron & Steel, Non-Ferrous products have become more complicated.ADCOAT has developed “Adpack-S”, Impregnated type VCI* paper (Anti-Corrosion Paper) in common use to protect them from rusting/corrosion.This is workable with higher performance for Iron & Steel, Non-Ferrous products such as Copper, Brass, Phosphor Bronze, Tin Plate Galvanized, Chromed, Nickel-plated with its feature of less deterioration (in color change) of plastics than conventional type.
    atribut:
    • For use: Iron, Steel, Aluminium, Cooper, Brass, Zinc, Tin, Chrome, Nickel
    • Length (m): 1
    • Size (m): 1x1
    • Type: Single Sheet
    • Width (m): 1
  4. Branofol VCI Anticorrosion Film
    Mulai

    Rp1.199.900

    Branofol VCI Anticorrosion Film
    Deskripsi:
    - Product Characteristics. BRANOfol M3 is a bluish transparent, nitrite-free, special-polyethylene foil, two-side active, with active VCI corrosion protection. It is waterproof, weldable and suitable for automatic packing as well as paper bag production. By emitting constantly a small amount of active anticorrosion substances (VCI principle: Volatile Corrosion Inhibitor), BRANOfol M3 helps to protect metal parts during transport and storage. Active VCI agents effuse and build up a protecting atmosphere, which protects reliably against rust, even after having opened the package for a short time - the protecting atmosphere can be rebuild immediately. The distance from the foil to the metal depends on the package volume and the time permitted for a protecting atmosphere to build up. A rule of thumb: 10cm. Advantages : - Corrosion protection without oiling and greasing. - Package and anticorrosion protection in one. - Metal parts are ready for use at any time. - Economy of time. - Simple disposal. - Low package requirements. - In accordance with TRGS 615. - Transparent package. - Sealable to bags, tubes. - Protects against humidity. - Non - hazardous material. - Good stretch ability and breaking strength. - Range of Protection. BRANOfol M3 protects steel, cast iron on contact, nickel, aluminium, chromium, zinc and copper and its alloys reliably against corrosion. Test is recommended for cadmium and magnesium and its alloys. Duration of protection: Depending on the climatic conditions and closeness of package, up to 12 month. For application advice, please contact your application specialist.
    atribut:
    • Size (m): 1x100
    • Tensile Strength (MPa): 19 (MD), 18 (CD)
    • Breaking Load (kN/m): 1.14 (MD), 1.08 (TD)
    • Elongation at Break (%): 550-650 (MD)
    • Water Vapour Transmission (g/m2xd): 1.7
    • Color: Blue
    • Thickness (µm): 60
  5. SANKO Hit Anchor Type C (Baut Angkur Ketok)
    50%
    Mulai

    Rp9.900

    SANKO Hit Anchor Type C (Baut Angkur Ketok)
    Deskripsi:
    Hit Anchor dari Sanko ini memiliki variasi ukuran 6-20 mm familiar digunakan oleh Semua industri termasuk konstruksi dan maintenance
    atribut:
    • Surface Treatment: Chromate treatment
  6. ARMOR Protective Packaging Plastik Anti Karat
    Mulai

    Rp1.599.900

    ARMOR Protective Packaging Plastik Anti Karat
    Deskripsi:
    ARMOR POLY® VCI FILMA Multifunctional Film for Multi-Metal ProtectionARMOR POLY® VCI film protects metal from the evils of rust and corrosion. Not only do they serve as a physical barrier against moisture and humidity, all ARMOR POLY films contain ARMOR’s proprietary VCI Nanotechnology™ (a.k.a., our “secret recipe” for vapor corrosion inhibitor). Once metal is enclosed or wrapped in ARMOR POLY, VCIs activate to form a superhero-like corrosion-inhibiting shield on the surface of the metal to repel rust.ARMOR POLY is a clean, dry and easy-to-apply packaging option for metal/metal parts. Available in rolls, sheets, bags, tubing and shrink film, ARMOR POLY VCI films are transparent, heat sealable, environmentally friendly and recyclable. As an added benefit, many of the ARMOR POLY films contain ARMOR’s Bright Idea Technology™ — under a black light they emit glowing visible proof that VCI is present.ARMOR products are in-stock and ready-to-ship with no order minimums through our ARMOR Stock & Ready® program.
  7. ARMOR Protective Packaging Metal Rescue Rust Remover Bath
    Mulai

    Rp249.900

    ARMOR Protective Packaging Metal Rescue Rust Remover Bath
    Deskripsi:
    Clean, Safe and Easy RPHistorically, companies have relied on oils, grease and solvents to prevent rust on metal or metal parts. No matter what the formulation, these rust prevention liquids (RPs) have come at a “cost” — a cost to the environment, a cost to the health and safety of employees, and at a cost to a company’s bottom line for their failure rate to prevent rust effectively.Armor Protective Packaging® has spent more than 40 years developing rust prevention methods that are clean, safe, easy and that “save” — save time, save money, and save metal/metal parts from damage and reworking.While ARMOR offers a full line of paper and poly film packaging materials that contain its VCI Nanotechnology™ (which stands for vapor corrosion inhibitor) to keep the surface of metal free from rust, ARMOR also offers its own water-based RP called Dry Coat.We at ARMOR found a way to make a “clean break” from the mess and hazards of oil/grease/solvent-based rust prevention by developing our own water-based RP that is easy to apply, dries quickly, isn’t sticky or tacky, and that protects ferrous metals stored indoors for up to one year — it’s our Dry Coat and Dry Coat ST Rust Preventative — Invisible Protection, Visible Results.
    atribut:
    • Product Form: Liquid
  8. ADPACK VCI Paper Continuous Roll AGKT- 6M
    Mulai

    Rp31.900

    ADPACK VCI Paper Continuous Roll AGKT- 6M
    Deskripsi:
    Adpack-G (Impregnated Type for Iron & Steel)European chemical substance regulation REACH/CLP compatible products Trust more than 50 years of experience. Passed the exam stipulated in JIS Z 1535It is a type of impregnated VCI paper on kraft paper. It is widely used mainly in applications such as steel, automotive parts, and mechanical parts, and has a track record from more than 50 years experience.
    atribut:
    • For use: Iron, Steel & Aluminium
    • Type: Continuous Roll
    • Width (m): 1
  9. ADPACK VCI Paper Single Sheet AGKT- 6M
    Mulai

    Rp15.900

    ADPACK VCI Paper Single Sheet AGKT- 6M
    Deskripsi:
    Adpack-G (Impregnated Type for Iron & Steel)European chemical substance regulation REACH/CLP compatible products Trust more than 50 years of experience. Passed the exam stipulated in JIS Z 1535It is a type of impregnated VCI paper on kraft paper. It is widely used mainly in applications such as steel, automotive parts, and mechanical parts, and has a track record from more than 50 years experience.
    atribut:
    • For use: Iron, Steel & Aluminium
    • Length (m): 1
    • Size (m): 1x1
    • Type: Single Sheet
    • Width (m): 1
  10. ADPACK VCI Paper Continuous Roll ASK - 6M
    Mulai

    Rp33.900

    ADPACK VCI Paper Continuous Roll ASK - 6M
    Deskripsi:
    Adpack-S (Impregnated for Ferrous & Non-Ferrous)Impregnated type for Iron & Steel, Non-Ferrous productsIron & Steel, Non-Ferrous products have become more complicated.ADCOAT has developed “Adpack-S”, Impregnated type VCI* paper (Anti-Corrosion Paper) in common use to protect them from rusting/corrosion.This is workable with higher performance for Iron & Steel, Non-Ferrous products such as Copper, Brass, Phosphor Bronze, Tin Plate Galvanized, Chromed, Nickel-plated with its feature of less deterioration (in color change) of plastics than conventional type.
    atribut:
    • Type: Continuous Roll
  11. ARMOR Protective Packaging Dry Coat Rust Prevention Spray
    Mulai

    Rp61.900

    ARMOR Protective Packaging Dry Coat Rust Prevention Spray
    atribut:
    • Packaging: Bottle
    • Volume (ml): 250
  12. ARMOR Protective Packaging Metal Rescue Rust Remover Gel
    Mulai

    Rp499.900

    ARMOR Protective Packaging Metal Rescue Rust Remover Gel
    atribut:
    • Packaging: Can
    • Volume (g): 500
    • Product Form: Gel
    • Volume (ml): 500
  13. Jembo Power Cable Thermoplastic NYAF Series For Building (Kabel Listrik)
    Rating:
    100% of 100
    (5)
    Mulai

    Rp27.900

  14. AS ONE Aluminized PET Film
    Mulai

    Rp1.099.900

    AS ONE Aluminized PET Film
    atribut:
    • Base Material: PET (polyethylene terephthalate)
    • Base Thickness (µm): 12
    • Evaporated Film Thickness (Å): about 10
  15. KAWAKAMI Bubble Wrap Polyethylene VCI-Puti (Plastik Gelembung)
    Mulai

    Rp6.299.900

    KAWAKAMI Bubble Wrap Polyethylene VCI-Puti (Plastik Gelembung)
    Deskripsi:
    -Putiputi which is laminated with rust preventive film.-Can save the time of double packaging of rust preventive material and cushioning material. -Packing for rust prevention, storage.-Metal products.
    atribut:
    • Thickness: 3.5mm
    • Structure: Three-layers Type
    • Material: Polyethylene (PE)
    • W x L: 1200mmx42m
  16. Wipro Oxygen Regulator (Regulator Las)
    Mulai

    Rp439.900

    Wipro Oxygen Regulator (Regulator Las)
    atribut:
    • Color: Green
    • Dimensions (cm): 15x10.5x14.5
  17. OKAY Printer Label
    Mulai

    Rp1.299.900

  18. Philips TL-D Standard Colours (Lampu TL-D)
    50%
    Rating:
    93% of 100
    (12)
    Mulai

    Rp17.900

    Philips TL-D Standard Colours (Lampu TL-D)
    Deskripsi:
    Lampu TL-D Standard Colors menciptakan suasana dari cahaya putih hangat hingga cahaya siang hari yang sejuk. Lampu dengan efektivitas dan renderasi warna menengah.Keuntungan:Menciptakan suasana dari putih hangat sampai dengan putih sejukAplikasi:Sesuai untuk digunakan dalam berbagai luminer untuk lampu neon TL-D, yang digunakan dalam sejumlah aplikasi yang tidak menjadikan renderasi warna sebagai faktor penting
    atribut:
    • Type: Standard
  19. Diversey Divodes Disinfectant
    Mulai

    Rp1.899.900

    Diversey Divodes Disinfectant
    atribut:
    • Volume (ml): 20000
    • Packaging: Pail
Daftar Harga kertas anti karat Terbaru November 2026
ARMOR Protective Packaging Kertas Anti KaratRp4.199.900
Multiguard VCI Anticorrosion FilmRp1.999.900
ADPACK VCI Paper Single Sheet ASK - 6MRp20.900
Branofol VCI Anticorrosion FilmRp1.199.900
SANKO Hit Anchor Type C (Baut Angkur Ketok)Rp9.900
ARMOR Protective Packaging Plastik Anti KaratRp1.599.900
ARMOR Protective Packaging Dry Coat Rust PreventionRp1.399.900
ARMOR Protective Packaging Metal Rescue Rust Remover BathRp249.900
ADPACK VCI Paper Continuous Roll AGKT- 6MRp31.900
ADPACK VCI Paper Single Sheet AGKT- 6MRp15.900

Data diperbarui pada 23/11/2026 (Harga belum termasuk PPN)